NX Creating a User Defined Cycle in Post Configurator to be used in NX

2022-07-05T12:36:43Z
NX for Manufacturing

Summary


Details

In Post Builder there was an option to create custom drill cycles using the Create New Machine Control Event utility. Is there a way to create these cycles in Post Configurator?



Solution

To create a User Defined Cycle in Post Configurator create a UDE and than change the EVENT header to CYCLE when copying the UDE event code into the ude.cdl
 


When a drilling operation is created the custom cycle is displayed from the Cycle menu.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: P2027
Function: POSTCONFIG

Ref: 001-10368036

KB Article ID# PL8651625

Contents

SummaryDetails

Associated Components

Manufacturing Post Builder Manufacturing Post Configurator