Create self populating drawing templates

2022-06-15T17:14:09Z

Summary


Details

How do you create/edit automatic text in NX Drafting?

Solution

To create self-populating annotation, the steps are as follows:


1. In the component of Master Model top level part file, create a attribute.  In the image below, I created "Piece" in the assembly file (component of the specification) and assigned the value "Bench Assembly".






2. In the top level (specification) file, I created an Attribute in the Attribute Templates dialog (File --> Utilities --> Attribute Templates) using the prefix DB_DWG_TEMPLATE_. This prefix is necessary for any attribute you want to auto-populate. Do not set a Default Value:



3. Create a Note using the Relationships option, select the Insert Object Attribute option and then select the Master Model assembly file:








Place the note on the drawing:





If you enter the attribute template in a Title Block of a drawing/sheet template file, it will update when the template is added to a Master Model:










Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V2007
Function: ANNOTATION

Ref: 001-10365104

KB Article ID# PL8650220

Contents

SummaryDetails

Associated Components