Face color changes when importing Parasolid file

2023-08-17T02:38:48Z

Summary


Details

After assigning a face color in NX, when exporting it to a Parasolid file and importing it back to NX, the face color changes.。

Reproduced Steps:

1.Create a solid and change some face color of the solid by "Edit Object Display"


2.File > Export > Parasolid( Reproduce with any option)

3.File > Import > Parasolid( Reproduce with any option)


Solution

This behavior is due to NX bug and has been fixed in NX 2027.3300.

Workaround:

Open the Parasolid file directly without using Import > Parasolid.

  -File> Open

Notes

This behavior only occurs in NX 2007 Series. In addition, it's the problem specific to the face, so there is no problem with other geometries such as a solid.

*** Please refer to PL8648427 for Japanese article.

Notes

KB Article ID# PL8648428

Contents

SummaryDetails

Associated Components