Missing geometry when loading jt model

2022-08-23T07:54:53Z

Summary


Details

When open a psz file, some cojt(jt) has display issue in Process Simulate, most of the geometry was disappeared.

But when open that jt file in Teamcenter Visualization, it indicates the jt file is fine, but it could not be displayed correctly in Process Simulate.

Solution

This is because the data contains a corrupted JT file.

To remove the corrupted data, do below steps:

1. Created a new empty study

2. Inserted the component to the study

3. Executed - open to modeling and end modeling

4. Exit from PS (no need to save the study)

Now when I load the study there are no missing geometry from other components.

However the resolution is not ideal as empty shapes are replacing the corrupted data, so some data was lost.

Please submit a support case.

Notes

Notes

KB Article ID# PL8642343

Contents

SummaryDetails

Associated Components