How to write a value to a data point via the deployment workflow

2022-05-24T21:44:46Z

Summary


Details

You are having difficulties with the deployment workflow to write a value to a data point. 

How can you achieve this?

Solution

There are two ways to write the value to the device.

option 1: This is a recommended option.

1)

GET API:

 

https://gateway.eu1.mindsphere.io/api/mindconnectdevicemanagement/v3/devices/Assetid/dataConfig   

This API is to get the data source id and data point id.

2)

Create a new job Instance (POST API)

https://gateway.eu1.mindsphere.io/api/deploymentworkflow/v3/instances

Here you need to provide the body.

Body:

{

"deviceId": "string",

"model": {

"key": "mdsp-core-commandDispatcher",

"customTransitions": []

},

"data": {

"type": "datapoint-write",

"createdBy": "user@company.com",

"to": "PROTOCOL_NAME",

"version": "v1.0",

"payload": {

"protocol": "PROTOCOL_NAME",

"desiredValue": "232",

"dataSourceId": "ID_OF_DS",

"dataPointId": "ID_OF_DP"

}

}

}

Option 2:

1)

GET API:

https://gateway.eu1.mindsphere.io/api/mindconnectdevicemanagement/v3/devices/Assetid/dataConfig   

This API is to get the data source id and data point id.

2)

Post to write a data point (POST API)

https://gateway.eu1.mindsphere.io/api/mindconnectdevicemanagement/v3/devices/{{AssetID}}/writeDataPoint

Body:-

{

"dataSourceId": "ID_OF_DS",

"dataPointId": "ID_OF_DP",

"desiredValue": "4"

}

Notes

KB Article ID# PL8642104

Contents

SummaryDetails

Associated Components