Adding colors to Color Manager

2022-05-12T11:37:09Z

Summary


Details

Is there a way to add colors to Color Manager? 



Solution

Yes.

The colors available in Color Manager are the default colors in the assembly. 
To create a new color, select the Styles button, choose Face Styles from the Style Type list, then click New. 
Give the new Face Style a Name on the Name tab, then select a color you want the new Face Style to be based on.

You can also base the new Face Style off No Style and create the new style from scratch. 
You can change the properties of the New Face Style on the Name, Edges , Faces, Texture, Bump, Appearance, and Reflection Box tabs.

The New Face Style will now appear under Styles -> Faces Styles.
Now go to Color Manager and see that your new Face Style is in the list. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10-20h2
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V221MP11
Function: DISPLAY

Ref: 001-10346323

KB Article ID# PL8641483

Contents

SummaryDetails

Associated Components