The stub orientation of the PMI datum feature symbol is inverted
2022-05-09T02:12:57Z
Summary
Details
The stub orientation of the "Datum Feature Symbol" placed on the stub of the leader line of the PMI dimension is inverted when the view is rotated. The stub orientation of the "datum feature symbol" placed on the leader line (not the stub portion) of the PMI dimension is not reversed.
Reproduced Steps:
1.Create 2 PMI dimensions. One is with a stub and another is with no stub 2.Create 2 Datum Feature Symbol on both of PMI dimensions to be created in Step.1 - 1."A" : on the leader line of PMI dimension - 2."B" : on the stub of (the leader line in) PMI dimension 3.Rotate the view( 180 degrees around Y axis ***The stub orientation of the "Datum Feature Symbol" placed on the stub of the PMI dimension is inverted.
Solution
This behavior is working as designed. Note that this is due to the specific limitations to "Datum Feature Symbols", and the stub orientation of other PMI geometries such as "Note" and "Feature Control Frame" is not reversed.
Notes and References
*** Please refer to PL8639540 for Japanese article.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: PMI Version: V1919 Function: ANNOT_PLANE