Adding Tap Deep Cycles to a Post Builder Post

2024-03-13T15:06:07Z

Summary


Details

There is no output in the NC code when posting a tapping cycle in Post Builder using Drill,Tap,Deep.

Solution

1. Add a Custom Command to the Start of Program with the following code:



TapDeepCycle.txt (703 Bytes)

2. Create a cycle_tap_deep block using N/C Data Definition -> Block -> cycle_tap -> Create -> cycle_step (Q – Step Incr Value) -> Add Word.


Turn on the Drill Tap Deep option in NX.


Notice the Q output.


Notes

KB Article ID# PL8639191

Contents

SummaryDetails

Associated Components