Solid Edge What are the abbreviations for the standards in the Standard Parts database?

2024-04-04T16:42:10Z
APPLICATION

Summary


Details

Do you work with Solid Edge Standard Parts and tend to load all parts during the installation?  If so, please keep in mind that we offer a lot of worldwide standards for our international customers.

For your reference, below is an overview of the standards we deliver.  Generally, there is no need to load all of them into your database.  To avoid an overloaded and slow database, we recommend to only load those standards your company needs and delete standards your company does not need, respectively.  You can always subsequently load any standards that are missing.

Solution

Here is a list of the shortcuts and where those standards come from:

ANSI American
ASME American
BS British
CNS Chinese
CSN Czech
DIN German
GB/T Chinese
GOST Russian
IS Indian
ISO International
JIS Japanese
KS Korean
UNI Italian

Notes

Notes

KB Article ID# PL8638822

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS