Which Standard Parts versions are delivered with Solid Edge?

2025-02-19T09:11:22Z

Summary


Details

We deliver Standard Parts with each version of Solid Edge, and it is always useful to know the version numbers and make sure to have the latest version installed.

Solution

With each Solid Edge version we deliver Standard Parts.  The version for the Standard Parts does not match the Solid Edge version.  If no modifications have been made the version number does not change.   Some Standard Parts need modifications either because the standard has changed or fixes were made to the parts.  If so, then those new parts get new version numbers.  The free content delivered when installing the Standard Parts Administrator with the option to install Master Parts has another version number to that of the parts delivered with the Machinery or Piping Library.

These are the corresponding version numbers:

Solid Edge version Standard Parts Standard Parts
Free content (Master Parts) Library parts (Machinery & Piping)
V19 7.45 7.5
V20 7.95 8.0
ST 8.45 8.5
ST2 8.95 9.0
ST3 9.95 9.5
ST4 9.95 10.00
ST5 10.45 10.50
ST6 10.95 11.00
ST7 11.45 12.00
ST8 12.95 13.00
ST9 13.95 14.00
ST10 14.95 15.00
2019 15.95 16.00
2020 16.95 17.00
2021 17.95 18.00
2022 18.95 19.00
2023 19.95 20.00
2024 23.95 24.00
2025 24.95 25.00

If you see issues with a certain Standard Part, make sure you have the latest version registered in your Standard Parts database.

Notes

More information in our Solid Edge Standard Parts FAQs collection

KB Article ID# PL8638561

Contents

SummaryDetails

Associated Components