Solid Edge
Unable to start Solid Edge Electrical Manager.
2022-04-25T14:09:57Z
APPLICATION
Summary
Details
Electrical Manager will not start. Fails with Error 1068: The dependency service or group failed to start.
Solution
- browse to C:\Program Files\Siemens - select Properties on the "Solid Edge Wiring and Harness Design 2022" folder - add System to have full control over security of the folder
** might need to add local admin and network admin
- start the Electrical Manager service
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: SOLID_EDGE Application: SE_ELECTRICAL Version: V222.0 Function: OTHER