In the small examples there are subfolders where all the objects for the system are contained. Customer would like to set this up for their project. It will allow them to create a MU at a station with the method control ~.UserObjects.Bonder.create(?). Otherwise, they can't navigate to the object since the frame and MU is not in the same root folder.
However, they can't get a user object to move down to the user folder they made. How do they accomplish this?
Solution
To move an object via drag and drop into another folder, you have to keep the Shift key pressed.
This is to prevent accidentally moving an object to a different folder.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V2201
Function: ALL
Ref: 001-10318258