Setting a Display Filter in the Operation Navigator has changed in NX2007

2022-04-06T21:11:24Z

Summary


Details

A Filter needs to be set in the Operation Navigator so that only the operations with the characters "TAP" in the name are displayed. The menu options to set this filter changed from NX1980 to NX2007. How do I set this Filter in NX2007?

In NX1980 the button picks are Column Header -> MB3 -> Create Filter -> By Name(Checked) -> *TAP* -> Apply.


Use Column Header -> MB3 -> Apply Filter to reset the view.



Solution

In NX2007 the button picks have changed. The selections are now Column Header -> MB3 -> Filter -> Contains -> TAP -> Apply.


Use Column Header -> MB3 -> Clear Filters to reset the view.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: CAM
Version: V2019
Function: USER_INTERFACE

Ref: 002-8634202

KB Article ID# PL8634202

Contents

SummaryDetails

Associated Components