Zooming when editing dimension

2022-04-11T18:05:30Z

Summary


Details

Trying to Zoom in and out while a dimension is selected and the value is changing. 



Solution

This will happen if the following Option is enabled: 
Application button -> Settings -> Options, General page -> Enable value changes using the mouse wheel.


While the mouse is over the dimension value box, the value will change, but as soon as you move out of the box, the Zoom function will be enabled. Uncheck this option and it will only zoom. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V222MP3
Function: DISPLAY

Ref: 001-10315431

KB Article ID# PL8633895

Contents

SummaryDetails

Associated Components