Unable to migrate SE2021 Standard Parts TC Managed to SE2022.

2022-04-04T14:09:07Z

Summary


Details

Unable to migrate SE2021 Standard Parts TC Managed to SE2022. 

Solution

Please see the File Attachment "Migration of older TC Standard Parts to 2022.docx". It presents suggested steps to migrate the standard parts from Solid Edge 2021 (Teamcenter enabled) to Solid Edge 2022.

In addition to this document, the following sequence might help:
1. Install Solid Edge on the machine designated for the Standard Parts Administrator.
2. Install the standard parts administrator. Do not install any libraries.
3. Install Solid Edge 2022 MP3.
4. Start 'Parts Management Administrator. It would have all fields blank.
5. If you specify the location of the Standard Parts configuration folder by selecting the network path from the old installation (i.e.  \\ServerName\STDParts), make sure to hit the ENTER key when you paste that string into this box. You should see the 'Database Migration' dialog at this time.
6. Click on 'Start'.
7. The new database should then be ready for use.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: APPLICATION
Version: V222MP3
Function: STANDARD_PARTS

Ref: 002-8633816

KB Article ID# PL8633816

Contents

SummaryDetails

Associated Components