Solid Edge Wiring Design - Grid visibility issue

2023-01-16T05:32:53Z

Summary


Details

Grids are not visible properly when zoom out while working with Solid Edge wiring design. Need to zoom on certain level to see grids.

SEWD_Set Grid.JPG (50.5 KB)

Solution

The grid points are shown only when the user has zoomed to a certain level. This is because these grid points are useful while drawing the objects or connections.

 

The size of the grid can be defined in the project preferences, where its default value is 0.25cm

 

The display size of the grid is controlled by the fact whether it is a major grid or a minor grid.

 

If the user wants to see the major grids, they can have a Major grid interval after every 2 grids. That would make major grids appear closer to each other whenever they would zoom to the objects.

 

Notes

10238493

KB Article ID# PL8633369

Contents

SummaryDetails

Associated Components