Plant Simulation Indirect Addressing (ExtendPath)

2022-03-30T17:16:40Z
Plant Simulation

Summary


Details

Is there anyway to make Indirect Addressing with ExtendPath work? Customer has done this before to point to various stations, but now they are trying to use it to point to a specific user-defined variable.
 
In the below example:
?.NextSta = String "To_OP90"




If they manually type it in the method it works, but referencing it via ExtendPath does not. 



Solution

If To_OP90 is an attribute of @ then this will work: 

@.setAttribute(?.NextSta, true) 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V2201
Function: ALL

Ref: 001-10312551

KB Article ID# PL8631449

Contents

SummaryDetails

Associated Components

Application Education Gantt Chart General Interface Package Professional Runtime Standard VSM Library