import_attr_mappings is not removing /master=iman

2023-10-27T13:31:08Z

Summary


Details

The /master=iman option is removed from an existing attribute, and the mapping file is re-imported. The mapping import is successful.
However if the mapping file is immediately re-exported, the /master=iman is back on the attribute.
The /master=iman option will not remove from the attribute.  

Solution

Is the attribute at the Item level or the Item Master Form level?

In the header of the mapping file, there is a note:
# NOTE: for item master form the qualifier master=nnn is reassigned to master=iman
# where nnn can be cad, both, or none.

===========================

This means that for attributes writing to the ItemMaster Form, any "/master=" entry (/master=cad, /master=both, /master=none) will be reassigned to /master=iman.

Since there is no "/master=nnn" entry on the attribute, the default is "/master=both". By removing the /master=iman entry in the attribute mapping, the default becomes /master=both (which again will be re-assigned back to /master=iman).

So if the attribute is mapped to the Item or ItemMaster form, the "/master=" entry will be re-assigned automatically back to /master=iman.

If you would like to enable the CAD data to write to an Item level object (such as the Item or ItemMaster form), you can set this Teamcenter preference: TC_NX_allow_attrsync_master_with_item=YES

(instructions below).

Once this above preference is set, then the attributes can have /master=cad, or /master=both. and write to the Item level object. You should now be able to remove the /master=iman from the attribute mapping and import the mapping file. On re-export of the mapping file, the attributes should no longer have the /master=iman qualifier.1. In Teamcenter, select 'Edit-->Options'.
2. Select the 'Filters' tab at the bottom of the page.
3. Add this Teamcenter preference as a Site preference: 
 TC_NX_allow_attrsync_master_with_item=YES

Notes

KB Article ID# PL8630130

Contents

SummaryDetails

Associated Components