Solid Edge What are the supported License Server operating systems for 2022

2024-08-05T04:11:53Z
PART/SHEETMETAL SETUP

Summary


Details

Which Windows Server versions are supported in Solid Edge 2022 Licensing? 

Solution

The supported versions are Windows Server 2019, Windows Server 2016, Windows Server 2012, and Windows Server 2012 R2. 

Notes

If you have further inquiries about floating Licensing please refer to the FAQs collection link below:

Solid Edge Floating License FAQs Collection


KB Article ID# PL8628503

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES