Teamcenter NX Templates issue

2022-12-23T11:15:48Z

Summary


Details

Unable to view Model templates in the File- New Dialog box

Solution

Customer has MFK settings, hence the MFK naming format need to be specified in the PAX files. Notes

The Customer template items are of type MFK.

The customer needs to modify their pax file entry if that contains a proper MFK id and not an item id for that palate entry.

e.g pax file entry for a MFK type is as follow

<PaletteEntry id="d2">

    <References/>

    <Presentation name="MFK9C1T1" description="MFK Case 1 Item Type. MFK=item_id">

        <PreviewImage type="UGPart" location="@DB/model-plain-1-mm-template/A"/>

    </Presentation>

    <ObjectData class="ModelTemplate">

        <Filename>@DB/%#MFK#%,=item_id=032364,object_type=MFK9C1T1/A</Filename>

               <Units>Metric</Units>

        <ItemType>MFK9C1T1, MFK9C1T2</ItemType>

        <RelationType>master</RelationType>

    </ObjectData>

  </PaletteEntry>

This helps to bring the Model templates into the File New Dialog.

Notes

KB Article ID# PL8627896

Contents

SummaryDetails

Associated Components