Ho do you save the settings on the Feature Callout tab of the Callout command?

2022-03-16T15:26:27Z

Summary


Details

Ho do you save the settings on the Feature Callout tab of the Callout command? 



Solution

These settings are actually stored in the Dimension Style, not the Callout command. Access the Styles dialog and set the Style Type at the top left to Dimension. Select the Style which you are using and click Modify. Go to the Feature Callout tab and set your desired settings. The next time a Callout is placed, it will use the appropriate settings. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V222.0
Function: ANNOTATIONS

Ref: 001-10295994

KB Article ID# PL8627428

Contents

SummaryDetails

Associated Components