NX
Representation of pillar only show top- and bottom-end in a drawing view.
2022-04-01T07:47:05Z
NX for Design
Summary
Details
A specific ship design pillar it's not represented fully on the drawing view. Creating a transversal view in ship design drawing and, in this frame, there is a pillar of specific type, then it's not represented. Only top- and bottom-end is visible, where the full length was expected.
Solution
Only the Top and End of the pillar is showing. This is caused by the configuration of the pillar in the spreadsheet. e.g. in pillar_round_mm.xlsx :
DisplayFlangeOnDrawing=FlangeEndOnly >> this will only show the Pillar-ends in the drawing.
Change to:
DisplayFlangeOnDrawing=FlangeFullLength >> this will show the full length of the Pillar on the drawing.