NX is Slow when Opening Operations and the NX Log shows the library_dialogs.prt being Repeatedly Loaded
2022-03-28T21:19:34Z
Summary
Details
In the log file NX reports that it is opening the library_dialog.prt part a large number of times. System performance is noticeably slow when opening operations. What could be causing this?
From the NX Log file notice that the library_dialogs.prt is being loaded again and again in the background:
Solution
One possible cause for this might occur if File -> Utilities -> Customer Default -> Manufacturing -> User Interface -> Dialog Boxes -> Always Update Dialog Boxes is checked. Uncheck this option and restart NX.
Notes and References
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: CAM Version: V2019 Function: USER_INTERFACE