Solid Edge Timestamp is added to property text for Teamcenter mapped date attributes.

2022-02-25T19:38:03Z
DOC_MANAGEMENT

Summary


Details

Solid Edge Date properties (Origination, Created) that are mapped to Teamcenter have a timestamp when they are added to drawings using Property Text. 



Solution

The problem is when the date is mapped to Teamcenter the timestamp is added to the date property. When the draft file is open and property sync occurs, the timestamp is pushed back into the Solid Edge property. In the mapping file make Master=CAD for the mapped date attribute. That will stop the timestamp from getting into the Solid Edge property. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V222.0
Function: SEEC

Ref: 001-10270027

KB Article ID# PL8617333

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC