NPT thread missing in Solid Edge Hole command

2022-04-22T14:10:22Z

Summary


Details

In the Solid Edge part environment, the American National Pipe Thread Standard (NPT) is missing in the Hole command.  How can I add these? 



Solution

When you place the Hole, select the 'Hole options'.

In the 'Standard' drop-down, make sure to select "ANSI Inch".

Under "ANSI Inch" NPT threads are listed.





Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V222.0
Function: FEATURES

Ref: 001-10280581

KB Article ID# PL8617017

Contents

SummaryDetails

Associated Components