Solid Edge Change computer for a Solid Edge subscription license

2024-08-05T06:21:16Z
PART/SHEETMETAL

Summary


Details

Is it possible to change the computer for a Solid Edge subscription license?

Solution

Yes, it is possible to change the computer.

For a subscription product, the license is downloaded from the web after activation. 

Re-activating the subscription license on another client is done via the Solid Edge License Utility, and entering the Activation code again.

Be aware that the re-activation using the same Activation code is only allowed a certain number of times, after which the customer will be blocked - it is like an Emergency license. 

If the customer wants to regularly move the license between different machines they should make it Cloud Enabled.  This is done on the siemens.com/gtac web page by selecting 'License management'. 

Here is the link to the License Management Page:

https://www2.industrysoftware.automation.siemens.com/LicenseManagement/Application

Notes

If you have further inquiries about Node Locked Licensing please refer to the FAQs collection link below:

Solid Edge Node Locked License FAQs Collection


KB Article ID# PL8616709

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES