A Post Configurator post is altered to output circular record motion with an R value instead of IJK. This is configured using the Circular Move Always with IJK setting. When posting the output is still IJK. What could be missing?
If the Turbo output is set to On the arc output will not use the R output. Instead it will use the IJK words will be output.
Instead of using the Turbo Mode On setting try using the Advanced option.
Notes
Notes