Postprocessor built in Postbuilder to be Encrypted

2022-09-13T05:10:39Z

Summary


Details

How to Encrypt the Postprocessor built in Postbuilder?

Solution

Post Configurator can be used to Encrypt the Postprocessor, either they are build in Post Builder or Post Configurator.

The following are the steps to Encrypt.

1. In NX go to Manufacturing Application. 

2. Select Post Configurator

Post Configurator Icon

3. In Choose Postprocessor dialogue box go to "Browse to Open or Encrypt".

  Make sure you select the right extension.(*.pui or *.psc), then select the postprocessor and select OK


4. If the Postprocessor is built in PostBuilder(*.pui). It will open the dialogue box of Encrypt Postprcoessor Files

5. Now you can Encrypt the Postprocessor with reference to Sold-To ID or Expiry Date.

6. A separate folder is created with the encrypted Postprocessors.

For more details on Encryption please refer to the documentation using below link.

https://docs.sw.siemens.com/en-US/product/209349590/doc/PL20200605195244930.mfgpostconfig/html/xid1855965   

Important Note: The Encrypted postprocessors are not supported in NX12 and below versions.

Notes

KB Article ID# PL8613916

Contents

SummaryDetails

Associated Components