I am unable to log in to the app via SSH.
SSH is enabled for space as well as for the application and I was able to generate ssh-code but getting access denied error. The same functionality was working before.
Could you please help us to resolve the issue ?. Attached is the error message below.
Solution
Please check the CF version it should be about 7 versions once you update the Cloud Foundry CLI next step try to use process guid so that you can connect via process guid.
To get the process guid below are the steps.
you can do the SSH using putty as well.
use the below command to SSH via putty
Notes
https://developer.mindsphere.io/paas/paas-cloudfoundry-ssh.html
For any questions or support in this matter, contact us through the support center.