Tecnomatix Process Simulate showing models in black color

2022-07-05T19:17:45Z
Process Simulate

Summary


Details

All object are now shown in dark color. They used to load normally. 



Solution

This is currently a common problem with the latest NVIDIA drivers (511.09 even with the 496.46, maybe others too). 
Our development is aware of that and they are just communicating this issue to the NVIDIA company so that the driver is fixed on their site. 
In the meantime, we recommend that you should use the following workaround.


Workaround: 
Set the OpenGL acceleration level to V4.1 and restart the Process Simulate. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V16.1.2.X
Function: PS_VIEWER

Ref: 001-10261153

KB Article ID# PL8613034

Contents

SummaryDetails

Associated Components

Process Simulate VC Lite