Solid Edge What information is needed to upgrade Node Locked License to SE401?

2024-07-30T17:18:10Z
PART/SHEETMETAL SETUP

Summary


Details

A customer has a Node Locked License of Solid Edge (Foundation, Classic or Premium).

Since we now offer customers with active Maintenance the ability to use Solid Edge CAM PRO 2.5 axes, the License of the customer needs to be updated. 

Which information has to be provided in order to get a valid License? 

Solution

Since CAM PRO has its origin in NX, the way of creating NX Node Locked licenses was different to Solid Edge Node Locked licenses.

In former times the Node locked License for CAM PRO was tied to the Mac Address from the Machine.

This has changed now.

Both products have to be combined in one License file and are tied now to the Composite2 ID

The customer therefore needs to provide the Machine Name and the Composite2 ID from the Machine, where Solid Edge and CAM PRO is installed, for the Solid Edge Product.

The ID  can be found with the Solid Edge License Utility:


Notes

Notes

If you have further inquiries about Solid Edge Node Locked Licensing please refer to the FAQs collection link below:

Solid Edge Node Locked Licensing FAQs Collection

KB Article ID# PL8612402

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FEATURES