Solid Edge How can spacing at the bottom of the plate be controlled in 2D Nesting?

2022-01-31T21:20:15Z
DRAFT

Summary


Details

How can spacing at the bottom of the plate be controlled in 2D Nesting?



Solution


There are only two ways to control distances between parts and the edge of the sheet in 2D Nesting at the moment:

1- Distance between parts is constant for all parts in the nest. It also applies to all sides of the parts, so it cannot be controlled for one particular part or a particular side of a part. This distance is controlled by the option Part Spacing;


2- The distance between parts and sheets can be controlled individually for the top, bottom, left and right sides of the sheet. The distance is the same between a side of the sheet and all parts that are placed against that side, meaning, all parts placed against the bottom of the sheet for example will be placed at the same distance as defined in the fields here.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: SE_2D_NESTING
Version: V222.0
Function: OTHER

Ref: 001-10252328

KB Article ID# PL8608533

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS