NX fonts are missing (only windows fonts, true type, notes annotation not available, iso-1)

2024-08-12T08:39:08Z

Summary


Details

In the fonts list of NX only windows fonts are listed.

Solution

The NX Fonts are still available. The out of the box value for the customer default to show them has been changed to Standard Fonts Only. 

 

To enable NX Fonts set the customer default Drafting->General/Setup->Miscellaneous->Fonts to Use to Standard and NX Fonts or NX Fonts Only.


Notes

The WYSIWYG text editor introduced in NX1980 Series does not support the NX fonts but the Windows Standard Font only.

Notes

KB Article ID# PL8607493

Contents

SummaryDetails

Associated Components