Where are themes stored.

2022-01-31T21:14:16Z

Summary


Details

Where are themes for Solid Edge stored? 



Solution

These are stored under the user's AppData folder. In the Windows Explorer address bar, key in %appdata% and this will take you to that folder. Then burrow down into Siemens\Solid Edge\Version XXX\Customization and you will find the delivered Solid Edge themes as well as any custom themes the user has created. By default, Solid Edge will find and incorporate these themes into the newer version installed on the same computer. For a new computer, you can copy these files from the old to the new computer. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10-1809
Product: SOLID_EDGE
Application: APPLICATION
Version: V222.0
Function: UI

Ref: 001-10249184

KB Article ID# PL8607287

Contents

SummaryDetails

Associated Components