- After selecting itemrevision in 4 tier rich client,
unable to create Solid Edge Draft (SE Draft) dataset.
- Error message of
No Ouput Data and No Exception
TC_KEEP_SYSTEM_LOG
to
1
then restarted Teamcenter Server Manager service (pool manager)
- After attempting the same operation, the tcserver syslog shows
... -1073741819: error_-1073741819 - Exception code: EXCEPTION_ACCESS_VIOLATION: ...
Solution
- Had to set each of the preferences
AIE_installed
AIE_em_installed
to default value of
OFF
- Afterwards, creation of the Solid Edge datasets in RAC was successful.
Notes