PLANAR TEXT : Single Line Fonts are not available in Note

2022-02-25T07:00:24Z

Summary


Details

The CAM operation Planar Text uses the Text created by Note to Machine(Engrave) Text on the Part.
The fonts like Chineset or Blockfont which are single line are helpful while creating single line toolpath.  They are not seen in the latest version.

How to get these Single Line Fonts?

Solution

The NX fonts are not shown because the out of box value of the Drafting->General/Setup->Miscellaneous->Fonts in Customer Default is set to "Standard Fonts Only".

To get the Single Line fonts set the Fonts to "Standard and NX Fonts" in the drop down.
Now you can see both types of fonts.

KB Article ID# PL8604016

Contents

SummaryDetails

Associated Components