Not able to save multiple sheets in Draft file to pdf format

2022-01-18T11:44:20Z

Summary


Details

Need to save draft files with multiple sheets to pdf format, but only one sheet is saved.



Solution

Go to the Save As command in Solid Edge, set the file type to .pdf and click the Options button. Check "Save all sheets." This will create a pdf with multiple sheets. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1511
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V221MP9
Function: PDF

Ref: 001-10240178

KB Article ID# PL8603644

Contents

SummaryDetails

Associated Components