NX What is the use of Local Namespace Output(ON/OFF) in Post Configurator

2022-02-25T06:58:22Z
NX for Manufacturing

Summary


Details

Need to know what is the use of Local Namespace Output(ON/OFF) in Post Configurator, When and how it should be used.

Solution

Local namespace output ON/OFF gives two different ways to generate output position
value of TCPM mode and Tilt Plane for 5axis machine.

 Local Namespace Output- OFF:

This switch the machine kinematics when tool path outputted with
TCPM mode or under Tilt Plane coordinate system.

No matter what real machine kinematics type is, for TCPM mode, machine kinematics type
always be set to 5_axis_dual_head.
For tilt plane mode (cycle800, G68.2, PANE SPATIAL) , machine kinematics type always be set to 5_axis_dual_table
Other kinematics setup are decided by group TCPM Kinematics and Tilting Plane Kinematics. 

KB Article ID# PL8603312

Contents

SummaryDetails

Associated Components

Manufacturing Post Builder Manufacturing Post Configurator