Solid Edge Can user control the page size of the output 3D PDF on the Solid Edge side?

2023-01-12T03:55:31Z
TRANSLATORS

Summary


Details

Can user control the page size of the output 3D PDF on the Solid Edge side.

For example, if user want to output in a vertically long size such as A4.

Solution

Solid Edge, 3D pdf does not have a paper size at all; it has a model space. It's a format to share your 3D design as a viewing format.

 

We don't think this is the intend of 3D pdf usage.

3D pdf is not a print format, it's a format to share your 3D design as a viewing format. If there are problems with printing than this is related to the printer driver and not the file format. The default size is 211.7 x 211.7 mm.

Like Solid Edge, 3D pdf does not have a paper size at all; it has a model space.  

Maybe the Adobe Acrobat Pro version has more options to create 3D pdf files. For Solid Edge we don't have any option to set.

Notes

10187158

KB Article ID# PL8602901

Contents

SummaryDetails

Associated Components

TRANSLATORS: OTHER