Solid Edge Some symbols and parts are missing in Solid Edge Wiring design

2023-01-12T03:47:54Z
APPLICATION

Summary


Details

1. While using Solid Edge Wiring design there are some symbols missing in symbol library. 

2.  While placing Device in Layout it shows error.

Solution

1. While using Solid Edge Wiring design there are some symbols missing in symbol library. 

- Apart from starter data, there are some versions 2 and 3 part and symbol libraries available on Support Center for download. If customer has not previously downloaded them, they can do it. Instructions are available in the same folders.

2. While placing Device in Layout it shows error.

- This might be because of symbols which are missing. Once user import the required library the error should not appear.

Notes

10184696

KB Article ID# PL8602894

Contents

SummaryDetails

Associated Components

APPLICATION: SE_ELECTRICAL