How to create a Cashew gate by using Gate Wizard?

2022-09-15T11:34:21Z

Summary


Details

How to create a Cashew gate by using Gate Wizard in Easy fill Advanced?

Solution

Step 1: Choose Easy Fill advanced tab→ Wizard group → Gate Wizard.

Step 2: Select the face you want to create a Cashew gate.

Step 3: In the Attribute group, in the Type of gate box, select a Cashew Gate.

Step 4: In the Attribute box, Choose as Cold Runner gate or Hot Runner Gate 

Step 5: In the Cross-Section Parameters group, in the Type box, Select a Circular type.

Step 6: In the D1 box, Enter a Diameter (D1) Value.

Step 7: In the D2 box, Enter a Diameter (D2) Value.

Step 8: In the d box, Enter a Distance (d) Value.

Step 9: In the w box, Enter a Width (w) Value.

Step 10: In the h box, Enter a Height (h) Value.

Step 11: In the Angle box, Enter Angle Value.

Step 12: Click Ok.

Notes

Notes

KB Article ID# PL8602712

Contents

SummaryDetails

Associated Components