Search the list of reasons set for TC_NX_CM_AutomatedDecision_Actions

2022-06-30T10:03:47Z

Summary


Details

Use of TC_NX_CM_AutomatedDecision_Actions 



Solution

Possible values are Released, NotModifiable, CheckedOutByAnotherUser, ManualCheckOutRequired (CICO policy is Manual or SuperManual only), and Effectivity Split. These reasons are associated with the current object state and the target under which the changes are being made. Only one value can be used.

Note: Here "ManualCheckOutRequired" option is applicable for both "Manual Check Out Required" and "Manual Check Out Required for BVR" messages.

Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10-20h2
Product: NX
Application: NXMANAGER
Version: V2007
Function: INTELLIGNT_SAVE

Ref: 001-10233478

KB Article ID# PL8602660

Contents

SummaryDetails

Associated Components