Cursor is jumping in graphics screen and will not snap to points on curve

2021-12-28T13:53:25Z

Summary


Details

Cursor is jumping in graphics screen and will not snap to points on curve.



Solution

If the user is using a Logitech device, there is a setting called Smart Move which can cause this behavior if it's enabled.  For example, the user was creating a Studio Spline and the cursor was jumping to the G1 G2 G3 constraint tab which appears when selecting a point for the spline.  This setting was also causing the cursor to jump to the lower right area of the graphics window when an alert message appeared.  Disabling this setting resolved the issue.  



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V1980
Function: GRAPHICS

Ref: 001-10231382

KB Article ID# PL8601421

Contents

SummaryDetails

Associated Components