About [Include Subassemblies] option for Parts List command.
2021-12-15T06:27:22Z
Summary
Details
About [Include Subassemblies] option for Parts List command.
Solution
From the Parts List. You need to be select the "Select Object" option when selecting the "Include subassembly" option.
Includes or excludes the components of a subassembly when it is selected from the Assembly Navigator or from the graphics window.
When "Include subassembly"; OFF The only subassembly is added in the Parts List. Refer below Image-1
Image-1 When "Include Subassembly"; ON The subassembly, as well as included components in subassemblies, are added in the Parts List. Refer below Image-2
Image-2.
Notes and References
10221505
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: DRAFTING Version: V1953 Function: TABLES