Custom templates not loading for users

2022-03-09T14:02:01Z

Summary


Details

Templates are not found in the 'File-->New' dialog.



Solution

If NX was launched from Active Workspace, check to make sure the NX role has access to the ItemTypes of the templates. 
The role used in Active Workspace may not be the same role used in NX. 
1. In NX, select 'File-->Preferences-->Teamcenter Integration'. 
2. Select the 'Database' tab. 
3. Change the role to a role that has access to the ItemTypes of the PAX files (if PAX files are stored in Teamcenter), the ItemTypes listed in the PAX files, and the ItemType of the template files themselves.

Active Workspace and NX do not synchronize roles, so it may be that the role in Active Workspace has access to the PAX files and templates, but the role of the user in NX does not.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: FILE_NEW

Ref: 001-10225785

KB Article ID# PL8600297

Contents

SummaryDetails

Associated Components