When a component is inserted from the Reuse Library, NX acts like it inserted, but nothing happens.
The user can browse the Reuse Library, select 'Insert' on a library part, enter all the options and the location to insert the component. NX acts like it is thinking about creating and inserting the component, but nothing happens.
Solution
Even though there is no error to the NX user, in the NX log was reported the following error:
****************************************
Teamcenter Error: 100101 (100101)
Explanation:
The ODS connection to site <> on host <> failed.
Program not registered
****************************************
Even though the ODS service was running, it needed to be recycled.
Recycle the ODS service and see if the component is now generated and inserted into the NX assembly successfully.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1953
Function: FILE_OPEN
Ref: 001-10228315