Newer revision information available after assembly loaded?

2022-02-09T21:05:05Z

Summary


Details

Using Assembly Load Options of 'Precise Only', a precise assembly is loaded into NX with certain specific revision of component opened along with it.


Once this precise assembly is loaded, how to indicate which of the components have newer revision existing in TC database? 



Solution

Use following steps to obtain information on which of the components have newer revision existing in TC database: 

(1) In Assembly Navigator, make sure the column 'TC Information' is turned on. 

(2) Position the cursor so it is NOT on top of any components (position over the navigator header area is good idea), then Right Mouse Button and choose 'Refresh Teamcenter Information'.


(3) Now examine the Assembly Navigator's 'TC Information' column for any yellow-triangular marker, existence of this marker indicate the component that has newer revision existing. By place cursor over the marker will reveal balloon of information including the latest revision ID that exists. 



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V1953
Function: ASSEMBLY_NAV

Ref: 001-10228568

KB Article ID# PL8600068

Contents

SummaryDetails

Associated Components