Plant Simulation
JT for PickAndPlace objects not getting transferred from TC to Plantsim using TC
2021-12-09T17:03:03Z
Plant Simulation
Summary
Details
In Plant Simulation 16.0.4.2123.
Customer is using Teamcenter Wizard in the PlantSim to transfer objects from Teamcenter to Plant Simulation. They have filled the "PlantSim class" attribute as PickAndPlace for an object in the Teamcenter MPP. Those objects JT is not getting transferred using Teamcenter Wizard in Plant Simulation.
Solution
The object '.Tools.TeamcenterWizard.ResourcePool.PickAndPlace' has a custom attribute with name 'ReplaceGraphicsWithTcJT' which is set to false per default: The reason is, the Plant Simulation PickAndPlace object has a kinematic defined. If you load the JT from TC it will be a static graphic.
If this is what you want, you just have to change the value to true.
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: TECNOMATIX Application: PLANTSIMULATION Version: V16.0 Function: ALL