An unexpected error occurred when importing the Solid Edge templates into Teamcenter.

2022-01-18T11:48:35Z

Summary


Details

An unexpected error occurred when importing the Solid Edge templates into Teamcenter. 



Solution

Here are a couple of things to look for when receiving errors adding templates to Teamcenter:


1. "Out of the box" properties Document Number, Revision, and Project Name (assuming using the default behavior where Project Name = Item Name) should be empty. Make sure that there is no custom property named Teamcenter Item Type. 

2. No custom properties that are related to Teamcenter, like a timestamp, should be showing when the file is loaded into Teamcenter via Add to Teamcenter. 

Preparing the template for upload as stated above should result in successful import.




Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V222.0
Function: SEEC

Ref: 001-10225131

KB Article ID# PL8599438

Contents

SummaryDetails

Associated Components