Solid Edge Cannot Balloon Certain Components in Assembly Drawing

2021-12-08T19:20:12Z
DRAFT

Summary


Details

Parts in assembly not showing up in parts list and balloon as "N/A" when manually ballooned. 



Solution

Go into the assembly. Right click on the part(s) in question and select Occurrence Properties. Scroll across to the column "Reports/Draft List" and make sure the value for that part is set to Yes. If set to No, these parts are ignored by the parts list and associated balloons. 



Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: 10-1909
Product: SOLID_EDGE
Application: DRAFT
Version: V222.0
Function: TABLES

Ref: 001-10225067

KB Article ID# PL8599076

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS